Boot Problem:FEC: Link is down 7949

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Problem:FEC: Link is down 7949

Jump to solution
10,023 Views
vishvapathi
Contributor V

finished compiling LTIB on Ubuntu 12.04. Copied bootloader, uImage and rootfs files in sdcard as per the LTIB document. When i power ON the EVB connecting via serial port getting below problem.

U-Boot 2009.08 (Jun 19 2013 - 15:09:12)                                
                                                                       
CPU: Freescale i.MX6 family TO1.2 at 792 MHz                           
Thermal sensor with ratio = 189   

Temperature:   33 C, calibration data 0x5ac4de7d

mx6q pll1: 792MHz                 
mx6q pll2: 528MHz                 
mx6q pll3: 480MHz                 
mx6q pll8: 50MHz                  
ipg clock : 66000000Hz

ipg per clock : 66000000Hz

uart clock: 80000000Hz
cspi clock: 60000000Hz                                                
ahb clock : 132000000Hz                                               
axi clock   : 264000000Hz                                                 
emi_slow clock: 132000000Hz                                               
ddr clock : 528000000Hz                                               
usdhc1 clock  : 198000000Hz                                               
usdhc2 clock  : 198000000Hz                                               
usdhc3 clock  : 198000000Hz                                               
usdhc4 clock  : 198000000Hz                                               
nfc clock : 24000000Hz                                                
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]                
Boot Device: SD                                                           
I2C:   ready                                                              
DRAM:   1 GB                                                              
MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3                
*** Warning - bad CRC or MMC, using default environment                   
                                                                          
In:serial                                                             
Out:   serial                                                             
Err:   serial                                                             
Found PFUZE100! deviceid=10,revid=11                                      
Net:   got MAC address from IIM: 00:04:9f:02:6c:a6                        
FEC0 [PRIME]                                                              
Hit any key to stop autoboot:  0                                          
PHY indentify @ 0x1 = 0x004dd074                                          
FEC: Link is down 7949                                                    
Using FEC0 device                                                         
TFTP from server 192.168.1.101; our IP address is 192.168.1.103           
Filename 'uImage'.                                                        
Load address: 0x10800000                                                  
Loading: FEC: Link is down 7949                                           
FEC: Link is down 7949                                                    
FEC: Link is down 7949                                                    

FEC: Link is down 7949

The above line is repeating continuously....

Did i do any mistake while compiling or copying it to SD card??



Labels (2)
0 Kudos
Reply
1 Solution
7,236 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi

       Please modify last sentence: bootcmd=run bootcmd_net .

        Change it to "bootcmd=run bootcmd_mmc"

save and exit, and re-complie u-boot. continue to test !

Regards,

weidong

View solution in original post

0 Kudos
Reply
13 Replies
7,236 Views
gurumoorthirasi
Contributor IV

your log saying that it is looking for the kernel image through network so change the ip to none and set the environmental variable to sdcard.then this will work.refer their Linux_user guide.pdf.

0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

Hi Guru,

  I tried to  Hit any key to stop auto-boot but not getting any response for any key press, its starting to display Link is down 7949 repeatedly.

When i insert the android SD card which came along it works fine. I dont think booting from SD is the problem, plz correct me if i am wrong...

0 Kudos
Reply
7,236 Views
weidong_sun
NXP TechSupport
NXP TechSupport

hello,Vishvapathi,

    Please use print command on u-boot command line to show u-boot environment , then paste them here. let us check them.

     It seems that settings is configured as booting from tftp and NFS. If it is like this, we should adjust environment or set up tftp and nfs on linux host.

Regards,

Weidong

0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

Hi Weidong,

    I am not getting the Uboot command line. the console starts printing FEC: Linik is Down 7949 continuously. I tried to  Hit any key to stop auto-boot but not getting any response for any key press, its starting to display Link is down 7949 repeatedly. When i insert the android SD card which came along it works fine

0 Kudos
Reply
7,236 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi,

      Please check the header file for your board, it should be in u-boot/include/configs/, Mine is mx6solo_sabresd.h, I can't confirm your file's name. find it and open it, then search "CONFIG_EXTRA_SETTINGS", all default environments parameters are defined here, so paste them here. Let me see .

     Then we modify default environment and continue to test !

Regards,

Weidong

0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

Hi,

#define    CONFIG_EXTRA_ENV_SETTINGS                    \

        "netdev=eth0\0"                        \

        "ethprime=FEC0\0"                    \

        "uboot=u-boot.bin\0"            \

        "kernel=uImage\0"                \

        "nfsroot=/opt/eldk/arm\0"                \

        "bootargs_base=setenv bootargs console=ttymxc0,115200\0"\

        "bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs "\

            "ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp\0"\

        "bootcmd_net=run bootargs_base bootargs_nfs; "        \

            "tftpboot ${loadaddr} ${kernel}; bootm\0"    \

        "bootargs_mmc=setenv bootargs ${bootargs} ip=dhcp "     \

            "root=/dev/mmcblk0p1 rootwait\0"                \

        "bootcmd_mmc=run bootargs_base bootargs_mmc; "   \

        "mmc dev 3; "    \

        "mmc read ${loadaddr} 0x800 0x2000; bootm\0"    \

        "bootcmd=run bootcmd_net\0"                             \


0 Kudos
Reply
7,237 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi

       Please modify last sentence: bootcmd=run bootcmd_net .

        Change it to "bootcmd=run bootcmd_mmc"

save and exit, and re-complie u-boot. continue to test !

Regards,

weidong

0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

Hi,

Thanks for your help. But now i am getting kernal image error. I loaded the uImage as per the document.

Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR]                
Boot Device: SD                                                           
I2C:   ready                                                              
DRAM:   1 GB                                                              
MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3                
*** Warning - bad CRC or MMC, using default environment                   
                                                                          
In:serial                                                             
Out:   serial                                                             
Err:   serial                                                             
Found PFUZE100! deviceid=10,revid=11                                      
Net:   got MAC address from IIM: 00:04:9f:02:6c:a6                        
FEC0 [PRIME]                                                              
Hit any key to stop autoboot:  0                                          
mmc3(part 0) is current device                                            
                                                                          
MMC read: dev # 3, block # 2048, count 8192 ... 8192 blocks read: OK      
Wrong Image Format for bootm command                                      
ERROR: can't get kernel image!                                            

MX6Q SABRESD U-Boot >


0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

And i am not able to type anything on the command line...

0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

still facing the kernel image problems after doing the env settings as per the document.

U-Boot 2009.08 (Jun 20 2013 - 15:29:29)                                   
                                                                          
CPU: Freescale i.MX6 family TO1.2 at 792 MHz                              
Thermal sensor with ratio = 189                                           
Temperature:   45 C, calibration data 0x5ac4de7d                          
mx6q pll1: 792MHz                                                         
mx6q pll2: 528MHz                                                         
mx6q pll3: 480MHz                                                         
mx6q pll8: 50MHz                                                          
ipg clock : 66000000Hz                                                
ipg per clock : 66000000Hz                                                
uart clock: 80000000Hz                                                
cspi clock: 60000000Hz                                                
ahb clock : 132000000Hz                                               
axi clock   : 264000000Hz                                                 
emi_slow clock: 132000000Hz                                               
ddr clock : 528000000Hz                                               
usdhc1 clock  : 198000000Hz                                               
usdhc2 clock  : 198000000Hz                                               
usdhc3 clock  : 198000000Hz                                               
usdhc4 clock  : 198000000Hz                                               
nfc clock : 24000000Hz                                                
Board: i.MX6Q-SABRESD: unknown-board Board: 0x63012 [POR ]                
Boot Device: SD                                                           
I2C:   ready                                                              
DRAM:   1 GB                                                              
MMC:   FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3                
In:serial                                                             
Out:   serial                                                             
Err:   serial                                                             
Found PFUZE100! deviceid=10,revid=11                                      
Net:   got MAC address from IIM: 00:04:9f:02:6c:a6                        
FEC0 [PRIME]                                                              
Hit any key to stop autoboot:  0                                          
mmc - MMC sub system                                                      
                                                                          
Usage:                                                                    
mmc read addr blk# cnt                                                    
mmc write addr blk# cnt                                                   
mmc erase blk# cnt                                                        
mmc rescan                                                                
mmc part - lists available partition on current mmc device                
mmc dev [dev] [part] - show or set current mmc device [partition]         
mmc bootpart [dev] [part] - show or set boot partition                    
mmc list - lists available devices                                        
                                                                          

MMC read: dev # 0, block # 2048, count 8192 ... Card did not respond to voltage!

MMC: block number 0x2800 exceeds max(0x0)                                 
0 blocks read: ERROR                                                      
Wrong Image Format for bootm command                                      
ERROR: can't get kernel image!                                            
MX6Q SABRESD U-Boot > printenv                                            
bootdelay=3                                                               
baudrate=115200                                                           
ipaddr=192.168.1.103                                                      
serverip=192.168.1.101                                                    
netmask=255.255.255.0                                                     
rd_loadaddr=(0x1300000)                                                   
netdev=eth0                                                               
ethprime=FEC0                                                             
uboot=u-boot.bin                                                          
kernel=uImage                                                             
nfsroot=/opt/eldk/arm                                                     

bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverp

bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; boom

bootargs_mmc=setenv bootargs ${bootargs} ip=dhcp root=/dev/mmcblk0p1 rootwait  

ethact=FEC0                                                               
bootfile=uImage                                                           
loadaddr=0x10800000                                                       
bootargs_base=setenv bootargs console=ttymxc3,115200                      

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev2;mmc read ${loadaddr} 0x800 m

bootcmd=run bootcmd_mmc                                                   
stdin=serial                                                              
stdout=serial                                                             
stderr=serial                                                             
bootargs=console=ttymxc3,115200 ip=dhcp root=/dev/mmcblk0p1 rootwait      
                                                                          

Environment size: 785/8188 bytes 


0 Kudos
Reply
7,236 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi,

      It seems that u-boot didn't read linux kernel . please try to adjust environment:

u-boot > setenv bootargs_mmc 'run bootargs_base bootargs_mmc;mmc dev2;mmc read ${loadaddr} 0x800 0x2000;bootm'

u-boot > save

-----------------------------------------------

<note: please notice which eMMC port you are using mmc dev2 means uSDHC3 port. If errors still exist, you can modify dev number>

Regards,

Weidong


0 Kudos
Reply
7,236 Views
vishvapathi
Contributor V

Hi Weidong,

If i modify dev no also getting same error.. below are the commands i issued to set env

setenv loadaddr 0x10800000

setenv bootargs_base 'setenv bootargs console=ttymxc3,115200'

setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait rw

setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev1;mmc read ${loadaddr} 0x800 0x2000;bootm'

setenv bootcmd 'run bootcmd_mmc'

saveenv

run bootcmd

for my mmcinfo command below is the response

mmcinfo

Card did not respond to voltage select!

Device: FSL_USDHC

Manufacturer ID: 0

OEM: 0

Name: Tran Speed: 0

Rd Block Len: 0

MMC version 0.0

Clock: 400000

High Capacity: No

Capacity: 0 Bytes

Bus Width: 1-bit

Current Partition for boot: Not bootable

i burned images to SD card as per the instruction in i.MX 6Dual/6Quad SABRE-AI Linux User's Guide


I am a newbie, plz correct me if i am wrong.


Thanks in advance

0 Kudos
Reply
7,236 Views
gurumoorthirasi
Contributor IV
  "bootcmd=run bootcmd_net\0"                         \

the above line in code change _net replace with _mmc .

  "bootargs_mmc=setenv bootargs ${bootargs} ip=dhcp " \        "root=/dev/mmcblk0p1 rootwait\0"

the above line change the ip=none.