Boot Order when using HAB with a DCD present

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Order when using HAB with a DCD present

Jump to solution
2,626 Views
传策薛
Contributor V

Can send me the document, I also want to use the hab?

0 Kudos
Reply
1 Solution
2,579 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent  Your some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,580 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I've sent  Your some comments directly.


Have a great day,
Yuri

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,924 Views
narkoskatona
Contributor II

Could you send also to me, please?

0 Kudos
Reply
2,579 Views
传策薛
Contributor V

Thanks a lot

0 Kudos
Reply