Boot Mode iMX6UL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,422件の閲覧回数
srcoolz
Contributor II

Hello,

If the Fuses are set to boot from NAND and BOOT_MODE set to 00 with resistors - is it possible to change the BOOT_MODE to 01 via resistors even if the Fuses and programmed.

If yes, isn't this a security issue where in someone can change the boot mode, and boot from for eg. SD Card and read all the data from NAND. 

Is there a way to prevent changing the Boot Mode once the Fuses have been programmed?

Thank you

Regards

Santhosh

ラベル(1)
0 件の賞賛
返信
1 解決策
2,102件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs, so it

is not possible to change boot mode.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,103件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Santhosh

If BT_FUSE_SEL = 1, all boot options are controlled by the eFUSEs, so it

is not possible to change boot mode.

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,102件の閲覧回数
srcoolz
Contributor II

Hello Igor,

Thank you for pointing me to correct section. 

Regards

Santhosh

0 件の賞賛
返信