Boot Linux from QSPI NOR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Linux from QSPI NOR

2,192 Views
nitigupta
Contributor I

Hi All,

I am working on imx6UL evk board. I want to boot linux from QSPI flash by putting zImage, device tree & rfs on QSPI only. Is there any good tutorial available for the same?

Any help is highly appreciated.

Thanks,

Niti

0 Kudos
Reply
1 Reply

1,541 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Niti,

You could take a look at the following document, which explains how to change the boot source and considerations:

Booting Linux from SATA on i.MX6Q SABRE AI.

You could also refer to a similar QSPI boot clarifications on Vybrid which use the same controller than the i.MX6X and verify what applies for the i.MX6UL:

Parallel QuadSPI

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply