Boot IMX8MM using USB serial port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot IMX8MM using USB serial port

1,435 次查看
ajita02
Contributor IV

Hi all,

We have a custom board which uses IMX8MM. I want to boot board using serial port. We dont have eMMC support on board. Also board is not booting through sd card slot.

Thanks,

Ajita
iMX8MMINI

标签 (1)
0 项奖励
回复
3 回复数

1,431 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ajita02,

I hope you are doing well.

Please make sure that you have used the correct commands. Please share the uuu commands that were used to flash the board and board schematics for further debugging.

Please make sure that boot mode and CFG pins are set correctly.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复

1,385 次查看
ajita02
Contributor IV

Hi @Dhruvit,

Is it possible to boot kernel image through UUU? Our board dont have emmc support and our SD card is not booting. What can be done in this case?

I made bootmode switch as "1010xxxxxx". I have built "imx-image-full". The image has been tested with imx8mm evk board.

Thanks,

Ajita

0 项奖励
回复

1,347 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ajita02,

I hope you are doing well.

UUU can boot u-boot and can flash kernel image and rootfs.

If emmc is not available, then one can flash kernel image and rootfs to sd card using uuu.

Please change the DIP switches to serial download mode.

Please use the below command.

uuu -b sd_all <imx-boot-*> <rootfs/imx-image-full image>

After flashing one can change DIP switches back to internal boot mode & SD card.

Thanks & Regards,
Dhruvit Vasavada

0 项奖励
回复