Boot Contact Pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot Contact Pins

1,858 次查看
DaviddeBethel
Fresh Out Contributor

Hi Folks,

 

Can anybody give me any advice on the best way to set up the boot contact pins on the IMX257?

 

I wish to know if they all MUST be connected or can I connect the ones corresponding to NAND Flash (which I am using) to high, whilst leaving the non-required pins as no-connect.  I know this is classed as floating and may not be a good idea.

 

Else, I must use pull down resistors, but I worry that this may affect the use of the peripherals associated with these pins, such as CSPI2.

 

Any advice would be most gratefully received

 

ddB

标签 (1)
0 项奖励
回复
2 回复数

1,782 次查看
OmarPighi
Fresh Out Contributor
yes this is interesting, but is there any tool to read/blow fuses status for prototipe and production?
0 项奖励
回复

1,782 次查看
Frias
Contributor IV

Hello David,

 

Instead of using the external IO you can use the e-fuses to determine how the SoC boots.

 

Best Regards,

Renato Frias 

0 项奖励
回复