Board bring up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board bring up

1,553 Views
ullasbharadwaj
Contributor III

Hello,

   I am working with i.MX 6 Solo X Sabre SD board and trying to bring up the board using custom built kernel, u-boot and RFS(with Buildroot). 

1. Where can we get the sources of MBR (Stage 1 Bootloader) ?

2. I need to know how to add commands to U-boot shell Ex: bootaux (codes are available, viz bootaux.c etc) since I am not    aware of U-boot compilation.

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,340 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Ullas,

You could take as reference Chapter 4 “Yocto Project Setup” and Chapter 5 “Image Build” of the “i.MX Yocto Project User's Guide” document for building a minimal image to boot the i.MX and then mounting a different Root File System.

Additionally, you could take a look at the following Community document, which implements something similar to your request (building to a different board):

https://community.nxp.com/docs/DOC-332807

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,340 Views
ullasbharadwaj
Contributor III

Hello Carlos,

         Thank you so much for the response.

         Currently I am using yocto for images of Linux Kernel, U-Boot and RFS. But i wanted to know how can I get my hands on the sources of Bootstrap code. This is in concern if I want to use a custom board and I need to change my bootstrap parameters.

0 Kudos
Reply