Board bring-up: Change imx6ul u-boot debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Board bring-up: Change imx6ul u-boot debug

5,730 Views
pyraohms
Contributor III

We are about to manufacture a first spin of a custom imx6ul board, based on the EVK's design. Our design differs that we have our debug port on UART3 instead of UART1 on the EVK. We need to change this in u-boot and in the Linux kernel, to be able to see that our boards are alive. How do we go about doing this?

The following files (downloaded from NXP/Freescales git) are used:

uboot-imx-rel_imx_4.1.15_2.1.0_ga

rel_imx_4.1.15_2.0.0_ga

The other thing is that our hardware designer has used i.MX Pins Tool 2.0 to generate iomux config files that needs to be a part of the bulds. We would like to configure our kernel for further development, but initially set some GPIO's using u-boot. How can we do this?

Information found is for other boards and endless searching in the forums have not been succesful, please help.

Many thanks

Labels (1)
Tags (4)
0 Kudos
Reply
6 Replies

4,740 Views
pyraohms
Contributor III

Thank you for your response.

I have changed uboot/include/configs/mx6ul_14x14_evk.h to 

#define CONFIG_MXC_UART
#define CONFIG_MXC_UART_BASE UART3_BASE

and replaced every "ttymxc0" in the file.

I am building uboot-imx-rel_imx_4.1.15_2.1.0_ga from source with make distclean / make mx6ul-14x14-evk_defconfig

The output from UART1 stops, but i can't see any activity on UART3.

0 Kudos
Reply

4,740 Views
igorpadykov
NXP Employee
NXP Employee

please check if uart3 clock is enabled in CCM_CCGR1 register.

Best regards
igor

0 Kudos
Reply

4,739 Views
igorpadykov
NXP Employee
NXP Employee

Hi Per

please refer to attached Porting Guide Chapter 1 Porting U-Boot.

For different uart example one can look at uart4 i.MX6Q Sabre AI :

linux imx6qdl-sabreauto.dtsi and uboot/include/configs/mx6qsabreauto.h :
#define CONFIG_MXC_UART_BASE    UART4_BASE
#define CONFIG_CONSOLE_DEV        "ttymxc3"

GPIOs can be set in uboot/board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,739 Views
pyraohms
Contributor III

Thank you for your quick answer. However, i cannot make it work.

uboot/include/configs/mx6qsabreauto.h does have:

#define CONFIG_MXC_UART_BASE UART4_BASE
#define CONFIG_CONSOLE_DEV "ttymxc3"

uboot/include/configs/mx6ul_14x14_evk.h does have:

#define CONFIG_MXC_UART
#define CONFIG_MXC_UART_BASE UART1_BASE

The inconsistency makes me confused. Should i put (in mx6_14x14_evk.h):

 

#define CONFIG_MXC_UART
#define CONFIG_MXC_UART_BASE UART3_BASE

#define CONFIG_CONSOLE_DEV "ttymxc2"

for UART3 to be configured as debug port?

0 Kudos
Reply

4,739 Views
igorpadykov
NXP Employee
NXP Employee

yes these changes are right for for uart3 to be configured as debug port.

Also please change kernel boot parameter: console=ttymxc2,115200

~igor

0 Kudos
Reply

4,739 Views
pyraohms
Contributor III

Is there any other configuration (in other files) that needs to be made in u-boot? How about the kernel?

Many thanks!

0 Kudos
Reply