Bluetooth not working MCIMX8M-EVK kit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth not working MCIMX8M-EVK kit

2,460件の閲覧回数
shabbirlimdiwal
Contributor I

Hi,

I am booting fsl-image-qt5-imx8mqevk-20180802213331.rootfs.sdcard from sd card on my imx8m-evk kit. The version of the linux image is imx-4.9.88-2.1.0-8mm_alpha. The board boots fine but seems like on board bluetooth is not working. I ran below commands to test bluetooth after boot, 

root@imx8mqevk:~# systemctl start bluetooth
root@imx8mqevk:~# bluetoothctl
Agent registered
[bluetooth]# devices
No default controller available
[bluetooth]#

Any idea why ? I am attaching logs during boot for your reference. 

Thanks,

Shabbir

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,119件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

what version do you use? pls check the release note, it seems the Bluetooth is not enabled in the default prebuilt image

0 件の賞賛
返信

2,119件の閲覧回数
shabbirlimdiwal
Contributor I

I am using imx-4.9.88-2.1.0-8mm_alpha image. Thanks !

0 件の賞賛
返信

2,119件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the 4.9.88 release note, for imx8M, Supports Murata 1CQ (QCA6174A) Wi-Fi/Bluetooth.For i.MX 8MQuad, it needs to add kernel parameter "pci=nomsi" to support Murata 1CQ Wi-Fi. for more detailed information about bluetooth, you can refer to the release note.

0 件の賞賛
返信