Bluetooth Disconnection Issue on imx8mp Board using bluetoothctl - Need Solution

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bluetooth Disconnection Issue on imx8mp Board using bluetoothctl - Need Solution

799件の閲覧回数
sivaci2754
Contributor I

Hi

Currently I'm working on imx8mp board there i working with bluetooth but issue is while connecting bluetooth it getting disconnect within few second, I'm using bluetoothctl for these tings i took HCI logs also from btmon. https://kodi.software/ https://dltutuapp.com/tutuapp-download/ 

Can anyone help me to solve this problem.

0 件の賞賛
返信
1 返信

783件の閲覧回数
ramprakash08
Contributor IV

It sounds like you're experiencing a disconnection issue with Bluetooth on your imx8mp board. This could be due to a variety of reasons, such as interference, power issues, or software bugs.

Firstly, you might want to check if there's any interference that could be causing the Bluetooth disconnection. This could be from other electronic devices, walls, or even certain types of lighting. Try moving your setup to a different location to see if the problem persists.

Another common cause of Bluetooth disconnection is power issues. Make sure that your imx8mp board is adequately powered and that there are no issues with your power supply.

If the problem still persists, it could be due to a software bug. You mentioned that you're using bluetoothctl and have taken HCI logs from btmon. It would be helpful if you could share these logs so that we can better understand the issue. You can post them here on the forum, making sure to remove any sensitive information.

0 件の賞賛
返信