what is the difference between bitbake -c compile -f linu-imx and bitbake linu-imx
whenI run bitbake -c compile -f linu-imx this command it executed succesfully but when I try to do bitbake linu-imx it fails
已解决! 转到解答。
Hello,
Please look at the following
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
Please look at the following
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you YuriMuhin_ng got the difference...
one more issue is when I do bitbake fsl-image-gui the .sdcard image is showing 880MB size. How can I reduce the rootfs. where as my zImage is 4MB only.
Hi,
the .sdcard image includes U-boot, kernel and file system.
It requires to remove non-needed packages in order to reduce file system.
Perhaps it would be better to use core-image-minimal configuration.
Regards,
Yuri.