Bitbake options

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,513件の閲覧回数
chandraevolute
Contributor V


what is the difference between bitbake -c compile -f linu-imx and bitbake linu-imx

whenI run bitbake -c compile -f linu-imx this command it executed succesfully but when I try to do bitbake linu-imx it fails

0 件の賞賛
返信
1 解決策
2,957件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at the following

Useful bitbake commands

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,957件の閲覧回数
chandraevolute
Contributor V

I tried to run core-image-minimal and it is running 3.14.28 version  instead if 3.14.38...the 3.14.28 does not support for 3.14.38

0 件の賞賛
返信
2,958件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at the following

Useful bitbake commands

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,957件の閲覧回数
chandraevolute
Contributor V

Thank you YuriMuhin_ng got the difference...

one more issue is when I do bitbake fsl-image-gui the .sdcard image is showing 880MB size. How can I reduce the rootfs. where as my zImage is 4MB only.

0 件の賞賛
返信
2,957件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

  the .sdcard image includes U-boot, kernel and file system.

It  requires to remove non-needed packages in order to reduce file system.

Perhaps it would be better to use core-image-minimal configuration.

Regards,

Yuri.

0 件の賞賛
返信