Hello community,
In Reference Manual of i.MX6Dual/Quad(IMX6DQRM.pdf) rev 4 09/2017,
It was modified CCM_CLPCR register field descriptions from IMX6DQRM.pdf rev3 07/2015.
But it seems some mistake,
1) Allocate same bit (bit 21) of following register bits.
* BYPASS_LPM_HS0
* BYPASS_MMDC_CH1_LPM_HS
2) Allocate same bit (bit19) of following register bits.
* BYPASS_LPM_HS1
* BYPASS_MMDC_CH0_LPM_HS
3) Why it has no description in B.1.19 CCM Revision History?
I checked a IMX6Solo/DualLite reference manual(IMX6SDLRM.pdf) rev3 and it have same problem.
Please suggest a correct field of this register.
Best regards,
Ishii.
已解决! 转到解答。
Yes, you are right, there is the error in the CCM_CLPCR register description in the i.MX6Dual/Quad Reference Manual Rev.4 document. The correct CCM_CLPCR bit fields description is given in the Rev.3 document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, you are right, there is the error in the CCM_CLPCR register description in the i.MX6Dual/Quad Reference Manual Rev.4 document. The correct CCM_CLPCR bit fields description is given in the Rev.3 document.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------