Big noise when SSI work in asynchronous mode.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Big noise when SSI work in asynchronous mode.

ソリューションへジャンプ
8,543件の閲覧回数
luwinbo
Contributor III

As shown in the schematic diagram attached, playback and capture are on two chips respectively. both of them work in the master mode, imx6q works in the slave mode, playback and capture can work normally, but sometimes there is sudden noise during playback. Looking at TXFS and TXD waveform through an oscilloscope, it is found that there is suddenly no data in the left or right channel when noise is produced, refer to the attachments tek1.png and tek2.png. The waveform without noise is shown in tek0.png.

If RXC/RXFS/RXD is disconnected, the playback will work perfectly, no noise generated, and tek1.png and tek2.png waveforms not generated.

The configuration I have made is as follows. Is there anything missing? If anyone can provide some guidance, it will be appreciated.

The BSP version 4.9.17, which is for android 8.0.0_1.0.0 of imx6, and the chip is imx6q.

/* in the dts, active fsl,ssi-asynchronous */
sound {
    compatible = "fsl,imx-dummy-audio";
    model = "dummy-audio";
    cpu-dai = <&ssi2>;
    audio-codec = <&codec>;
    asrc-controller = <&asrc>;
    audio-routing =
        "Ext Spk", "SPK_LP",
        "Ext Spk", "SPK_LN",
        "Ext Spk", "SPK_RP",
        "Ext Spk", "SPK_RN",
        "CPU-Playback", "ASRC-Playback",
        "Playback", "CPU-Playback",
        "ASRC-Capture", "CPU-Capture",
        "CPU-Capture", "Capture";
    mux-int-port = <2>;
    mux-ext-port = <4>;
    codec-master;
    gpr = <&gpr>;
};

&ssi2 {
     assigned-clocks = <&clks IMX6QDL_CLK_PLL4>,
                  <&clks IMX6QDL_PLL4_BYPASS>,
                 <&clks IMX6QDL_CLK_SSI2_SEL>;
     assigned-clock-parents = <&clks IMX6QDL_CLK_OSC>,
                 <&clks IMX6QDL_CLK_PLL4>,
                 <&clks IMX6QDL_CLK_PLL4_AUDIO_DIV>;
     assigned-clock-rates = <1179648000>, <0>, <0>;
     fsl,ssi-asynchronous;
     status = "okay";
};


/* in the audmux, TXC/TXFS/RXC/RXFS get from external port */

     ret = imx_audmux_v2_configure_port(int_port,
        IMX_AUDMUX_V2_PTCR_TFSEL(ext_port) |
        IMX_AUDMUX_V2_PTCR_TCSEL(ext_port) |
        IMX_AUDMUX_V2_PTCR_RFSEL(ext_port | 0x8) |
        IMX_AUDMUX_V2_PTCR_RCSEL(ext_port | 0x8) |
        IMX_AUDMUX_V2_PTCR_TFSDIR |
        IMX_AUDMUX_V2_PTCR_TCLKDIR |
        IMX_AUDMUX_V2_PTCR_RFSDIR |
        IMX_AUDMUX_V2_PTCR_RCLKDIR,
        IMX_AUDMUX_V2_PDCR_RXDSEL(ext_port));
     if (ret) {
        dev_err(&pdev->dev, "audmux internal port setup failed\n");
        return ret;
    }
    imx_audmux_v2_configure_port(ext_port,
        0,
        IMX_AUDMUX_V2_PDCR_RXDSEL(int_port));
    if (ret) {
        dev_err(&pdev->dev, "audmux external port setup failed\n");
        return ret;
    }

/* in the codec dai, set symmetric_rates = 0*/
static struct snd_soc_dai_driver imx_dummy_codec_dai = {
    .name = "imx-dummy-codec-hifi",
    .playback = {
         .stream_name = "Playback",
         .channels_min = 1,
         .channels_max = 2,
         .rates = imx_dummy_codec_RATES,
         .formats = imx_dummy_codec_FORMATS,},
    .capture = {
         .stream_name = "Capture",
         .channels_min = 1,
         .channels_max = 2,
         .rates = imx_dummy_codec_RATES,
         .formats = imx_dummy_codec_FORMATS,},
         .ops = &imx_dummy_codec_dai_ops,
        .symmetric_rates = 0,
    };

0 件の賞賛
返信
1 解決策
8,298件の閲覧回数
luwinbo
Contributor III

This issue has been solved. It's a hardware issue. The reason is that RXC/RXFS/RXD interferes with TXFS signal, which makes SSI unable to recognize TXFS signal correctly.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
8,299件の閲覧回数
luwinbo
Contributor III

This issue has been solved. It's a hardware issue. The reason is that RXC/RXFS/RXD interferes with TXFS signal, which makes SSI unable to recognize TXFS signal correctly.

0 件の賞賛
返信
8,298件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lu

if this is just one board that may be soldering issue. In general one can try

with nxp linux bsps not using model = "dummy-audio", for example with

    sound {
        compatible = "fsl,imx6q-sabresd-wm8962",
               "fsl,imx-audio-wm8962";
        model = "wm8962-audio";..

https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/boot/dts/imx6qdl-sabresd.dtsi?h=i...imx6qdl-sabresd.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
8,298件の閲覧回数
luwinbo
Contributor III

Hi, Igor

Thanks for your comment, the dummy-audio is a driver written by my own, it works fine when SSI works in synchronous mode, so may I ask you a question, to the wm8962 audio driver and the ssi/audmux driver, what's the difference when SSI works in synchronous mode and the asynchronous mode?

0 件の賞賛
返信
8,298件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi lu

in synchronous mode, the transmit and receive sections of SSI share a common

clock port (STCK) and frame sync port (STFS).

In asynchronous mode, the transmitter and receiver each has its own clock and frame

synchronization signals.

Best regards
igor

0 件の賞賛
返信
8,298件の閲覧回数
luwinbo
Contributor III

Hi igor

Would you mind pointing out what I am missing according to the modifications I listed before.  thanks a lot.

Best regards.

Lu Winbo

0 件の賞賛
返信