Benchmarking Tools & Tests for IMX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Benchmarking Tools & Tests for IMX8QXP

2,337 Views
rvalvekar
Contributor III

Hello,

I am trying to get the phoronix test suite working with IMX8QXP Evaluation Board. I am just curios if anyone has used this test suite or any other tests suites for Benchmarking the System ?

Any Suggestions for Benchmarking Tools and Tests ?

From Phoronix Test Suite, some of the tests work with the hardware, not all. 

Thanks for the help,

Regards.

0 Kudos
Reply
2 Replies

2,244 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rohan

nxp does not provide benchmaring data, one can look at boundary devices

tests and try to reuse for i.MX8QXP

Nitrogen8M - Android Benchmark - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,244 Views
rvalvekar
Contributor III

Thank You Igor.

0 Kudos
Reply