Battery sizing using SNVS_LP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Battery sizing using SNVS_LP

1,558件の閲覧回数
ScottKerstein
Contributor III

Document Number: AN4509 Rev. 0, 09/2012 "i.MX 6Dual/6Quad Power Consumption Measurement" App Note states "The power consumption of SNVS is comparatively negligible except in Deep Sleep Mode” and doesn’t go into any more details

“Negligible” is a fuzzy word for something that is always on when coin cell is attached (SNVS_LP.) 

There must be some current which will help to size the battery as how long the need to have backup.

Are there any characterization results?

Thanks, in advance,

Scott

ラベル(1)
0 件の賞賛
返信
1 返信

1,469件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  To estimate battery options, please use “Stop Mode Current and Power Consumption” table

(SNVS Only mode) in the i.MX6 Datasheet(s), since in this mode supply current is provided by

battery.

 

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

 http://cache.nxp.com/files/32bit/doc/data_sheet/IMX6DQAEC.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信