Hello, the camera we use is OX0x8B (camera) + OAX4000 (ISP module) of OmniVision, which receives the signal of the OAX4000 through the MIPI-CSI interface of SOC (IMX8MQ) (parameter is 3840x2160@30fps, rate 1.2Ghz, format is YUV422, arrangement is YUYV)
I grab a frame of data such as an attachment (colorbar), what could be the reason?
The original image looks like this