Based on i.mx7ulp porting LPDDR2 SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Based on i.mx7ulp porting LPDDR2 SDRAM

3,315 Views
sam_liu
Contributor II

Hello everyone,

  I'm new here,could you give me a few pointers with LPDDR2 SDRAM porting.

  In my project, it's base on i.mx7ulp and the original Yocto BSP is set for LPDDR3.
Now I want to change the LPDDR3 to LPDDR2(1G) for my project's design, I already use the LPDDR2_RegisterProgrammingAid_V0_2.xlsx to create LPDDR2 relate setting register parameter in RealView.inc file.

According to "I.MX BSP Porting Guide " I already do some edit but I still have some question as below :

1. Whether I only need according to the register setting sequence and value in RealView.inc fill all parameter into the "imximage.cfg file" and then rebuild : bitbake -f -c compile u-boot-imx ?

Is there any files need to modify for porting SDRAM form LPDDR3 change to LPDDR2 ?

2. If the register setting sequence in imximage.cfg file is not match RealView.inc file , it will lead to an error or not?

3. Does the mx7ulp_evk.h file need to modify?

4.The //PCC0 ,//PCC1 and //PCC2 relate register setting in "RealView.inc file" are all set to value: 0x40000000 , whether I don't need fill these setting into imximage.cfg file?

5. The plugin.S file in git/board/freescale/mx7ulp_evk need to modify or not ? Does this file will be used when u-boot in boot phase?

Thank~

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,923 Views
sam_liu
Contributor II

Dear igorpadykov

  Can I ask you to do me a favour? I already fill in  LPDDR2 parameters into "imximage.cfg" refer to  "linux/board/freescale/mx7ulp_arm2  imximage_lpddr2.cfg" as you mentioned previously, but now I face another problem is the u-boot stuck and it doesn't show any message at UART port on my_customer board during boot stage. 

  Because my_customer board is boot from uSD-Card, so I measured both  "CLK" and "DATA0" signals  on uSD-card to confirm u-boot process is fail.

  I find that "CLK" and "DATA0" signals will continue normal active on NXP-EVB during boot stage (fig 1.) ,but  both these two signal on my_ customer board only active at the beginning during boot stage and then will STOP (fig 2.) . 

nxp_evb.jpg

                  fig 1 . Red : DATA0  Green: CKL on  NXP -EVB during boot stage.

  

my_board.jpg

                    fig 2 . Red : DATA0  Green: CKL on  MY- Board during boot stage.

 these are  what I modified in BSP as below : 

 1. change setting in  "mx7ulp_evk.c" uart port to match my_customer board design. 

 2. imx7ulp.dtsi(in U-boot) (for match my_customer design)

 3. imx7ulp-evk.dts(in U-boot) (for match my_customer design)

 4. imximage.cfg. 

 5. And I re-build "bitbake u-boot-imx" with no error.

 My question is shown as below :

 1. Actually ,relate to porting DDR process in the "i.MX BSP Porting Guide" only mention in chapter  "3.2.1 Changing the DCD table for i.MX DDR initialization "  , it's just indicate that we need to modify my_board.cfg.

I really want to known is HOW should I do to fill in DCD table parameters  refer to RealView.inc ?

Is these any document can show  more detail about modify the DCD table?

 2. Whether the modified of device tree  in u-boot source file will cause a u-boot fail?

    ( The modified "u-boot-imx" image  doesn't show any error message when I re-build it . ) 

 3. According to fig 2. wave form ,could you give me some tips about this case ? Is the DCD table configuration mistake cause this case ?or device tree configuration mistake in u-boot source code?

Thanks.

0 Kudos
Reply

2,923 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sam

example of lpddr2 configuration can be found in

linux/board/freescale/mx7ulp_arm2  imximage_lpddr2.cfg
https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7ulp_arm2?h=imx_v2017.03...
plugin.S file is not needed if plugin mode is not used (more description can be found in Boot

Chapter of Reference Manual).

>Does the mx7ulp_evk.h file need to modify?

no

>Is there any files need to modify for porting SDRAM form LPDDR3 change to LPDDR2 ?

except *.cfg file, in  linux/arch/arm/mach-imx  there are specific for memory low power codes
https://source.codeaurora.org/external/imx/linux-imx/tree/arch/arm/mach-imx?h=imx_4.9.88_2.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,923 Views
sam_liu
Contributor II

Dear igorpadykov

Thanks for your help, you do gave me a big favor. 

0 Kudos
Reply