BT1120 video input support on i.MX 6 or 8/9 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BT1120 video input support on i.MX 6 or 8/9 series

跳至解决方案
16,210 次查看
JK_Cha
Contributor IV

Hi iMX Champ

My customer would like to interface BT1120 video input based Camera Module along with iMX series.

Is there an iMX product to interface with BT1120 video format camera?
If not, is it recommended to use BT1120 to MIPI CSI bridge? I'd like to hear your opinion.

If possible, I would like to recommend you to design the iMX8 or 9 series.

Thanks.

Best Regards, 

Jacky

0 项奖励
回复
1 解答
16,198 次查看
joanxie
NXP TechSupport
NXP TechSupport

what TVIN chip do you use? I think you need TVIN support on imx series, right? imx6 and imx8 can support this, you can refer to the enclosed file

you also can refer to the link as below

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...

 

在原帖中查看解决方案

7 回复数
16,177 次查看
JK_Cha
Contributor IV

how about i.MX 93 serise for BT1120 de-interlace?

If not available from i.MX 9, then I would suggest customer to use i.MX 8M series.

0 项奖励
回复
16,158 次查看
joanxie
NXP TechSupport
NXP TechSupport

I confirmed that imx8qxp and imx93 only support BT656, if you must use BT1120, maybe you need choose imx6, for more detailed information, you can refer to the AN I sent to you before

0 项奖励
回复
16,174 次查看
joanxie
NXP TechSupport
NXP TechSupport

because imx93 is still under preproduction, I need double confirm it, but refer to the reference manual,— 8-bit/10-bit Camera Sensor Interface (CSI), so maybe only supports BT656, for the imx8qxp, I will also confirm it, because the patch I sent to you is for BT656, and the RM only mentions BT656, I need double confirm if imx8qxp parallel camera port can support this or not, wait for my update

0 项奖励
回复
16,183 次查看
JK_Cha
Contributor IV

And TVIN chip is not determined yet.

0 项奖励
回复
16,181 次查看
joanxie
NXP TechSupport
NXP TechSupport

ok, after you decide, maybe we can offer more detailed information, current imx8m series also can support de-interlace if you need BT1120 interlaced video

0 项奖励
回复
16,190 次查看
JK_Cha
Contributor IV

Hi Joanxie

Thanks for your kind answer.

I understood that we should use video decoder chip such as adv7180 etc. for BT1120 input, and I will deliver it to customer as difficult without external BT1120 to MIPI-CSI or Parallel bridge support.

Thanks.

Regards, 

Jacky

0 项奖励
回复
16,199 次查看
joanxie
NXP TechSupport
NXP TechSupport

what TVIN chip do you use? I think you need TVIN support on imx series, right? imx6 and imx8 can support this, you can refer to the enclosed file

you also can refer to the link as below

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/ISL79987-and-adv7180-de-interlace-driver...