Hi iMX Champ
My customer would like to interface BT1120 video input based Camera Module along with iMX series.
Is there an iMX product to interface with BT1120 video format camera?
If not, is it recommended to use BT1120 to MIPI CSI bridge? I'd like to hear your opinion.
If possible, I would like to recommend you to design the iMX8 or 9 series.
Thanks.
Best Regards,
Jacky
已解决! 转到解答。
what TVIN chip do you use? I think you need TVIN support on imx series, right? imx6 and imx8 can support this, you can refer to the enclosed file
you also can refer to the link as below
because imx93 is still under preproduction, I need double confirm it, but refer to the reference manual,— 8-bit/10-bit Camera Sensor Interface (CSI), so maybe only supports BT656, for the imx8qxp, I will also confirm it, because the patch I sent to you is for BT656, and the RM only mentions BT656, I need double confirm if imx8qxp parallel camera port can support this or not, wait for my update
Hi Joanxie
Thanks for your kind answer.
I understood that we should use video decoder chip such as adv7180 etc. for BT1120 input, and I will deliver it to customer as difficult without external BT1120 to MIPI-CSI or Parallel bridge support.
Thanks.
Regards,
Jacky
what TVIN chip do you use? I think you need TVIN support on imx series, right? imx6 and imx8 can support this, you can refer to the enclosed file
you also can refer to the link as below