BT1 and RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BT1 and RTC

5,697件の閲覧回数
JamesRobinson
Contributor II

Hello Group,

I just got my tablet today and the first thing that I noticed was that the RTC was not being updated between resets. I downloaded the HW docs and I see a reference to BT1. It looks like it should be located under the i.mx53 and to the right. But on my Rev, there is nothing there.

Can someone point me to the location of the RTC battery.

Thanks,

James

Board Info.

MCIMX53SMD

SCH-26876 REV D

700-26876 REV B

0 件の賞賛
返信
4 返答(返信)

5,603件の閲覧回数
i_Mx53
Contributor II

Hi James,

Now your time is remembering on the system,If we poweroff the tablet.When we on the tablet it is giving the correct time.RTC is working fine.

Please share me the picture of the backup battery with markings.

Thanks

-Nag

0 件の賞賛
返信

5,603件の閲覧回数
JamesRobinson
Contributor II

Update,

 Found the battery after I removed the main smd board. It is now located on the bottom of the board instead on top next to the processor. I also found it took more than a day on charger to get the battery to keep the battery running.

-James

0 件の賞賛
返信

5,596件の閲覧回数
JamesRobinson
Contributor II

Your image is where I thought it should be. 

Here is a picture of my board. I am a green board and not blue. It looks like they have updated the boards and not the docs on the freescale site.  Where BT1 should be I have u7......

-James

0 件の賞賛
返信

5,596件の閲覧回数
i_Mx53
Contributor II

Hi James,

Attach I am sending to you an image where you can see where you can add the LICELL coin battery. I hope this clarify.

Thanks,

Nagaraju

0 件の賞賛
返信