BT HFP workflow for buses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BT HFP workflow for buses

1,758件の閲覧回数
vinothkumars
Senior Contributor IV

Dear NXP,

 

Please provide the document for BT HFP workflow for Android 9 Automotive to IMX8 board.

By default alsa uses the audio_policy_configuration_car.xml . As per this configuration input device is mic and output device is bus0 or bus1.

 

Thanks & Regards,

 

Regards,
Vinothkumar Sekar
ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,722件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

You need to review in the schematics of the board that you are using which channel of the PCM of the Bluetooth it is use in order to configure in ALSA the workflow that maybe selected.

By default in our boards we only configure the codec to be the input and output, since Bluetooth it is not in our hardware board, it is externally added, like a module that need to be handle as an external audio board and in the configuration of Gstreamer or ALSA select the proper channel to get the HFP working

You may contact the Bluetooth manufacturer or the Bluetooth module in order to see if the option it is available.

0 件の賞賛
返信

1,718件の閲覧回数
vinothkumars
Senior Contributor IV

Thank you jamesbone

 

Sure I will check with vendor also.

Is it possible please share the HFP working log. It's good for debugging more.

 

Thanks,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信

1,746件の閲覧回数
vinothkumars
Senior Contributor IV

Why HFP voice is not getting from WM8960 (bus1_system_media_out)

 

Regards,

Regards,
Vinothkumar Sekar
0 件の賞賛
返信