Hello,
We are currently trying to make the BT.656 mode works on a iMX6Q. We use a custom driver, a custom baord, with a SOM.
I will explain all the configuration done, and the errors recieved:
On the .dtsi file :
pinctrl_ipu2_csi1: ipu1grp-csi0 {
fsl,pins = <
MX6QDL_PAD_EIM_A24__IPU2_CSI1_DATA19 0xb0b1 // Y/C[0]
MX6QDL_PAD_EIM_A23__IPU2_CSI1_DATA18 0xb0b1 // Y/C[1]
MX6QDL_PAD_EIM_A22__IPU2_CSI1_DATA17 0xb0b1 // Y/C[2]
MX6QDL_PAD_EIM_A21__IPU2_CSI1_DATA16 0xb0b1 // Y/C[3]
MX6QDL_PAD_EIM_A20__IPU2_CSI1_DATA15 0xb0b1 // Y/C[4]
MX6QDL_PAD_EIM_A19__IPU2_CSI1_DATA14 0xb0b1 // Y/C[5]
MX6QDL_PAD_EIM_A18__IPU2_CSI1_DATA13 0xb0b1 // Y/C[6]
MX6QDL_PAD_EIM_A17__IPU2_CSI1_DATA12 0xb0b1 // Y/C[7]
MX6QDL_PAD_EIM_A16__IPU2_CSI1_PIXCLK 0xb0b1 // Clk
//DATA_EN pin
MX6QDL_PAD_EIM_DA10__GPIO3_IO10 PAD_CTRL_HYS_PU //Unused
MX6QDL_PAD_EIM_DA11__IPU2_CSI1_HSYNC PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA12__IPU2_CSI1_VSYNC PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA5__IPU2_CSI1_DATA04 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA4__IPU2_CSI1_DATA05 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA3__IPU2_CSI1_DATA06 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA2__IPU2_CSI1_DATA07 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA1__IPU2_CSI1_DATA08 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_DA0__IPU2_CSI1_DATA09 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_EB1__IPU2_CSI1_DATA10 PAD_CTRL_HYS_PD
MX6QDL_PAD_EIM_D21__IPU2_CSI1_DATA11 PAD_CTRL_HYS_PD
>;
};
We are using the BT656 pins, (DATA19 to DATA12), other pins are declared but set in pull down, DATA_EN is set in pull-up, our fpga on the board, also set a +3V3 on this pin.
In the .dts:
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <0>;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};driver {
compatible = "driver,driver_camera";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu2_csi1 &pinctrl_cam0_gpio>;
clocks = <&clks 200>;
clock-names = "csi_mclk";
csi_id = <1>;
mclk = <148500000>;
mclk_source = <0>;
power-gpio = <&gpio3 19 0>;
status = "okay";
};
A FPGA is connected to the CSI pins, the FPGA seems to send valid data, with embedded sync.
Our driver works with mxc_v4l2_capture, and sets the following parametters:
.if_type = V4L2_IF_TYPE_BT656_PROGRESSIVE,
.mode = V4L2_IF_TYPE_BT656_MODE_BT_8BIT,
.bt_sync_correct = 0,
.nobt_vs_inv = 0,
.nobt_hs_inv = 0,
.pixelformat = V4L2_PIX_FMT_YUYV,
I put some debug in drivers/mxc/ipu_capture.c, when I run a pipeline I get the CSI registers :
[ 107.782327] CSI_SENS_CONF = 0x00000920
[ 107.786096] CSI_SENS_FRM_SIZE = 0x0437077F
[ 107.790197] CSI_ACT_FRM_SIZE = 0x0437077F
[ 107.794227] CSI_OUT_FRM_CTRL = 0x00000000
[ 107.798241] CSI_TST_CTRL = 0x00000000
[ 107.801906] CSI_CCIR_CODE_1 = 0x00040030
[ 107.805846] CSI_CCIR_CODE_2 = 0x00000000
[ 107.809773] CSI_CCIR_CODE_3 = 0x00FF0000
The CSI is in BT656, 8bpp, YUYV. 1920*1080, with the FF0000 embedded sync.
When the driver start :
[ 6.098746] mxc_v4l2_master_attach: ipu0:/csi1 parallel attached driver:mxc_v4l2_cap0
I think I have something wrong, I use IPU2 but mxc_v4l2 says I'm using IPU0, how do I change this? I tried to modify the ipu_id in the dts, but the slave is not found.
Also, when I run a gstreamer pipeline, I get a ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
I'm on 3.14 kernel, building images with Yocto, on poky branch.
Thanks for the Help,
Best regards,
Pierre-Olivier
已解决! 转到解答。
I checked some registers :
- IOMUXC_GPR1 bit 20 is set to 1 ( ipu2 connected to CSI1 not MIPI)
- IPUx_CONF is set to 0x80000002 -> CSI1 enabled and selected
- CCM_CCGR3 : 0x3ff3000f ->Clock of IPU2 not enabled, I tried to write 0x3ff30fff but it does not work. (I think this register is only for display)
- I removed the DATA_EN pin from the DTSI, as seen on this forum.
- I checked all the Pins, all are set to the right values, the daisy chain is set too.
- I tried to put IPU in TEST MODE, CSI_TEST_CTRL set to 0x01000000
With all these modifications, I still get ERROR: v4l2 capture: mxc_v4l_read timeout counter 0.
Any Thoughts?
EDIT:
I set CCM_CCGR3 register ipu2_ipu_clk_enable to 0x11 (always on), but when I load my driver, this register come back to 0x3ff3000f (disbaling the ipu2 clk)
Is this normal? I do not touch it in my driver.
EDIT2:
The configuration is right, SAV/EAV were in bad format.
I checked some registers :
- IOMUXC_GPR1 bit 20 is set to 1 ( ipu2 connected to CSI1 not MIPI)
- IPUx_CONF is set to 0x80000002 -> CSI1 enabled and selected
- CCM_CCGR3 : 0x3ff3000f ->Clock of IPU2 not enabled, I tried to write 0x3ff30fff but it does not work. (I think this register is only for display)
- I removed the DATA_EN pin from the DTSI, as seen on this forum.
- I checked all the Pins, all are set to the right values, the daisy chain is set too.
- I tried to put IPU in TEST MODE, CSI_TEST_CTRL set to 0x01000000
With all these modifications, I still get ERROR: v4l2 capture: mxc_v4l_read timeout counter 0.
Any Thoughts?
EDIT:
I set CCM_CCGR3 register ipu2_ipu_clk_enable to 0x11 (always on), but when I load my driver, this register come back to 0x3ff3000f (disbaling the ipu2 clk)
Is this normal? I do not touch it in my driver.
EDIT2:
The configuration is right, SAV/EAV were in bad format.
Hi Pierre-Olivier
for progressive BT.656 camera input one can look at below threads
https://community.nxp.com/thread/328880
https://community.nxp.com/thread/300234
https://community.nxp.com/thread/314211
ipu_id is configured in gpr1 register, one can try to debug it using
sect.6.3 Source Code Structure attached Linux Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, Thanks for the answer,
I tried to modify my DTS, I use IPU2_CSI1 so :
v4l2_cap_0 {
compatible = "fsl,imx6q-v4l2-capture";
ipu_id = <1>; // instead of 0;
csi_id = <1>;
mclk_source = <0>;
status = "okay";
};
I also modified the mach-imx.c, adding regmap_update_bits(gpr, IOMUXC_GPR1, 1 << 20, 1 << 20);
I checked, and this register is set, but when my driver starts :
[ 5.959969] mxc_v4l2_master_attach: ipu(0:1)/csi(1:1)/mipi(0:0) doesn't match
Ths slave IPU is 0(so IPU1), and master is 1(IPU2).
Where do I set the slave IPU correctly?
EDIT
I forgot to add the ipu_id in my driver, now I have [ 6.128704] mxc_v4l2_master_attach: ipu1:/csi1 parallel attached driver:mxc_v4l2_cap0
But When I run a gstreamer pipeline : [ 37.363757] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
Or when I do a cat /dev/video0 :
[ 440.503757] ERROR: v4l2 capture: mxc_v4l_read timeout counter 0
[ 440.509721] imx-ipuv3 2800000.ipu: Not a CSI channel
cat: read error: Timer expired
Any thoughts?
suggest first to check with imx-test (suggested links give examples of usage),
folder ../mxc_v4l2_test
I'm trying to build it with Yocto, but I get errors (I'm on Poky branch) when I add it to my image.
I tried to add the recipe for imx-test on Jethro branch, it compiles, but I only have the scripts, the binaries are not on my rootfs (mxc_v4l2_capture.out for example)