BSP sourceCode download link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BSP sourceCode download link

2,313件の閲覧回数
Harris
Contributor III

How to find a Linux 3.14 or Linux 4.1 BSP sourceCode download link.

In the following link, there is not a BSP sourceCode。

Embedded Linux for i.MX Applications Processo|NXP

Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,000件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

2,000件の閲覧回数
Harris
Contributor III

Hi, igor,

Thanks.

0 件の賞賛
返信

2,000件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

With BSP you  use Yocto Project with repo utility to fetch all the sources (layers) and then, in the process of building an image, you fetch the source packages, build them, etc.

But NXP source code is in http://git.freescale.com/git/

Follow the instructions in Freescale_Yocto_Project_User's_Guide.pdf document to build an image.

Luis

0 件の賞賛
返信