BOOT FOR MIMXRT1176DVMAA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOOT FOR MIMXRT1176DVMAA

3,104件の閲覧回数
bipul-jain
Contributor I

MIMXRT1176DVMAA Using this microprocessor how can i boot for very first time since i dont have any acces tp on board ROM and flash as MPU is not programmed

0 件の賞賛
返信
8 返答(返信)

3,078件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @bipul-jain ,

Thanks for your interest in NXP MIMXRT series!

Are you using NXP's EVK/EVKB or are you using a custom board?

 

0 件の賞賛
返信

2,963件の閲覧回数
bipul-jain
Contributor I

HI,@Gavin_Jia 

WE ARE MAKING A CUSTOM BOARD USING MIMXRT1176DVMAA

0 件の賞賛
返信

2,959件の閲覧回数
bipul-jain
Contributor I

@Gavin_Jia  ALSO WE ARE PLANNING TO ADD JTAG FOR DEBUG PLEASE HELP IN THAT TOO

0 件の賞賛
返信

2,960件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @bipul-jain ,

May you please refer to the answer of @julie598doyle ?  Thanks!

0 件の賞賛
返信

2,958件の閲覧回数
bipul-jain
Contributor I

bipuljain_0-1733814885144.png

@Gavin_Jia  we will use this circuit taken fron EVB kit 

so we have to keep our boot setting to inernal Boot Mode?

0 件の賞賛
返信

2,931件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

There is no problem with choosing internal boot, especially on prototype boards. However, in real products it is generally the case that Fuse boot is used, as this saves GPIO resources. Preserving the boot mode switching option is also something to consider. In short, design serves the product.

0 件の賞賛
返信

3,071件の閲覧回数
julie598doyle
Contributor I

Hello,
To boot the MIMXRT1176DVMAA for the first time without access to on-board ROM and flash, you can use an external debugger like J-Link. Connect it to your microprocessor and use it to load your initial program into the flash memory. This will allow you to start programming and debugging your device.

Best Regards,
Julie Doyle

0 件の賞賛
返信

2,956件の閲覧回数
bipul-jain
Contributor I

@julie598doyle  So We Have To Keep Our Boot Setting To Inernal Boot Mode In That case ?

0 件の賞賛
返信