BLE interfacing with i.MX6 over UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLE interfacing with i.MX6 over UART

1,068 Views
rahulsoni
Contributor II

Hi NXP Team,

We have a device in which we are using MCIMX6L8DVN10AA processor.We want to add BLE functionality into the device.For this, we are planning to use CC2640 Bluetooth Smart IC.

In CC2640 only 2 UART lines (RX and TX) are available for communication.

In processor, we have free UART (J19,J21,T20, T21) for UART (Tx, Rx, RTS & CTS lines) to communicate with CC2640 Smart IC.

My Query is:

Is UART 3 HCI Based?

Is there any necessary to use all 4 pins of UART for communicating with CC2640 or we can go for only 2 pins of UART (Tx & Rx) for communication by disabling Flow control

Labels (2)
0 Kudos
Reply
1 Reply

961 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rahul

in general it is not necessary to use all 4 pins of UART, but flow control

allows to achieve more fast and reliable communication with peripheral.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply