Availability of Unused Camera Parallel interface lines as GPIO's

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Availability of Unused Camera Parallel interface lines as GPIO's

跳至解决方案
928 次查看
harishs
Contributor I

Hi,

I would like to know whether the unused lines in 20 bit camera parallel interface of IMX6 Quad core processor can be used as normal GPIO lines. In my case i am interfacing a 10 bit monochrome image sensor to D19 to D10 lines of CPI interface.The data will be captured in 16 bit generic mode,my query is whether the unconnected 6 LSB bits when data is acquired in 16 bit generic mode can be used as normal GPIO lines. 

Regards,

Harish.S

标签 (1)
0 项奖励
回复
1 解答
853 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  yes, it is possible to configure the unused Camera interface pins for GPIO.

When configuring GPIO, Pin tools  may be useful.

Pins Tool for i.MX Application Processors|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
1 回复
854 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  yes, it is possible to configure the unused Camera interface pins for GPIO.

When configuring GPIO, Pin tools  may be useful.

Pins Tool for i.MX Application Processors|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复