Auto-Login and run a script Automatically

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto-Login and run a script Automatically

1,576 Views
m4l490n
Contributor V

Raybiztech‌ what if my board does not have the autologin script in /usr/bin? How can I achieve this?

0 Kudos
Reply
1 Reply

1,385 Views
b36401
NXP Employee
NXP Employee

Alternatively you can add the application into some startup script like /etc/rc.local.
However you need to make sure that all required services of the system are already running at the time the application starts.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply