Auto-Login and run a script Automatically

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Auto-Login and run a script Automatically

1,588 次查看
m4l490n
Contributor V

Raybiztech‌ what if my board does not have the autologin script in /usr/bin? How can I achieve this?

0 项奖励
回复
1 回复

1,397 次查看
b36401
NXP Employee
NXP Employee

Alternatively you can add the application into some startup script like /etc/rc.local.
However you need to make sure that all required services of the system are already running at the time the application starts.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复