Auto-Login and run a script Automatically

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Auto-Login and run a script Automatically

1,559件の閲覧回数
m4l490n
Contributor V

Raybiztech‌ what if my board does not have the autologin script in /usr/bin? How can I achieve this?

0 件の賞賛
返信
1 返信

1,368件の閲覧回数
b36401
NXP Employee
NXP Employee

Alternatively you can add the application into some startup script like /etc/rc.local.
However you need to make sure that all required services of the system are already running at the time the application starts.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信