Audio-in-out on imx6qp board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio-in-out on imx6qp board

2,057 Views
sachinarora
Contributor I

Hello,

We are using imx6qp SabreSD eval board (with OREO 8.0) to make a call. We are able to call the other person, but "Not able to hear or speak on the mic port and audio-out port."

Kindly note that we are able to play an audio file and listen to it using the audio-out port. Also, we are able to record the audio using the mic port on the kit.

Kindly help.

 

Thanks and Regards,

Sachin Arora

Labels (2)
0 Kudos
Reply
3 Replies

1,616 Views
smohsin
Contributor I

There are a few things that could be causing this issue. First, make sure that the audio levels are turned up on both your computer and your microphone. If that doesn't work, try plugging the microphone into a different port on your computer. If you're still having trouble, it's possible that there's an issue with your sound drivers. Try updating them or reinstalling them to see if that helps. mamc 

0 Kudos
Reply

1,965 Views
cisawohi
Contributor I

Hi buddy, did you get any permanent solution? As at my end the issue is more or less same. If you get any do let me know.

Regards,

Cisa Smith

_________________

https://plex.software/ https://tutuappx.com/ Vidmate

0 Kudos
Reply

1,965 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Have you installed in the proper way the extended media codecs?

Android OS for i.MX Applications Processors | NXP 

Embedded Application Software - miscellaneous

For more detail on it, please, refers to the i.MX Android Extended Codec Release Note

Best regards,

Diego.

0 Kudos
Reply