Audio Routing through HDMI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Audio Routing through HDMI

1,523件の閲覧回数
himanshugusain
Contributor III

Hi

We are using the customized SabreSD board running on android Lollipop

we are having issue w.r.t audio routing

the audio is always getting routed through HDMI

irrespective of the device connected or not

Hence we are not able to hear any audio in headphone/speaker

even though HDMI not connected .

How do we set audio routing to overcome this situation

Regards

Himanshu

ラベル(4)
0 件の賞賛
返信
1 返信

1,359件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi himanshu

for Lollipop sound routing one can look at

http://stackoverflow.com/questions/29671343/android-5-and-audio-routing

http://stackoverflow.com/questions/30101811/force-audio-routing-to-speaker-and-optionally-route-to-b...

it may be useful to check that in Linux:

Tips to fix sound server issues on linux (Alsa, Pulseaudio) ~ ShellScreen: Linux tuning, software, n...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信