Audio DDR frequency on iMX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Audio DDR frequency on iMX6ULL

1,507 Views
samuelrythm
Contributor I

Hello,

We are trying to save power on our iMX6ULL custom platform during lower computation periods. The idea would be to reduce DDR frequency which is a high power consumption budget.

We have tried to use low power idle DDR frequency mode (24MHz) but it is too slow for our computations, we cannot reach real time target.

We would like to run an intermediary DDR frequency (100MHz?) which seems to be named as "Audio DDR frequency" on Linux User guide (see below)

• Normal DDR frequency – Default frequency in U-Boot
• Audio DDR frequency – 50 MHz on i.MX 6Quad, i.MX 6DualLite, and i.MX 6SoloX, 100 MHz on i.MX 6SoloLite,
and 100 MHz on i.MX 7Dual
• Low power idle DDR frequency – 24 MHz
• Ultra Low power IDLE DDR frequency – 1 MHz (only on i.MX 6SoloLite)

However, iMX6ULL specific intermediary frequency does not appear on this document (L4.1.15_2.0.0-ga). Is document out of date?

When we try to force driver to pass into "Audio DDR frequency", DDR frequency stays at its default value (400MHz). Is iMX6ULL DDR controller able to run at an intermediary frequency? If yes, why isn't it available on current BSP? If not, is the limitation HW or SW?

Thank you for your help.

Sam

0 Kudos
Reply
1 Reply

1,367 Views
b36401
NXP Employee
NXP Employee

This document is a bit outdated in point of list of processors.
Please refer to chapter 24 "Dynamic Bus Frequency Driver" of i.MX Linux Reference Manual you can get from L4.1.15_2.0.0_LINUX_DOCS bundle.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply