Hi,
I am using 4 SPI ports of i.MX6UL. These signals are travelling from CPU board to base board and approximate distance is 20 CM. Let me know if I need buffer IC to drive signals strength of SPI signals. SPI is running on 3.3V.
The max. operating frequency of SPI would be 26MHz.
Regards,
Surendra
Hello,
As usually, the situation depends on environment : how PCB traces
are implemented; what cable , connector is used. To be completely accurate,
You need to perform signals simulation to check their integrity.
Buffers may be recommended in order to be fully on safe side.
Have a great day,
Yuri
------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer
button. Thank you!
Let me add few more things to above query.
The each SPI has only one slave connected to it. I also have provision to add buffer on base board.
Regards,
Surendra