Attach event detect in USB Host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Attach event detect in USB Host

Jump to solution
2,520 Views
ko-hey
Senior Contributor II

Hi all

I want to confirm a USB behavior, when I use USB as Host

When D+/D- goes High before initialization, can I detect Attach event ?

I read those following descriptions but there are no explanations.

"65.4.3.1 Host Controller Initialization"

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf

Ko-hey

Labels (2)
1 Solution
2,352 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your reply.

I understood like this. Is it correct ?

Since the detection of attach event before the initialization has been defined by the standard so i.MX6 also can be detected.

Ko-hey

View solution in original post

0 Kudos
Reply
6 Replies
2,352 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

in general attach event can be detected before

full usb controller initialization, please look at

sect.66.2.4.5 USB Plugged-In Detector IMX6DQRM

Description for attach event can be found

in sect.7.1.7.3 Connect and Disconnect Signaling usb 2.0

specification.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,353 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your reply.

I understood like this. Is it correct ?

Since the detection of attach event before the initialization has been defined by the standard so i.MX6 also can be detected.

Ko-hey

0 Kudos
Reply
2,352 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

what is:  "I understood like this. Is it correct ?" ???

~igor

0 Kudos
Reply
2,352 Views
ko-hey
Senior Contributor II

Igor

I apologize for any confusion.

I mean following sentence.

Since the detection of attach event before the initialization has been defined by the standard so i.MX6 also can be detected.

Ko-hey

2,352 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

yes correct

Best regards

igor

0 Kudos
Reply
2,352 Views
ko-hey
Senior Contributor II

Igor

Thank you !

Ko-hey

0 Kudos
Reply