Asynchronous operation(clEnqueueMapBuffer) is not working properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Asynchronous operation(clEnqueueMapBuffer) is not working properly

1,014件の閲覧回数
tetsuro-okuyama
Contributor V

Hi,

When executing clEnqueueMapBuffer, I want to set the argument blcoking_map=CL_FALSE to make it work asynchronously, but it only works synchronously.
When using OpenCL with i.MX8Mplus, does this function behave in accordance with the OpenCL specifications? Or are there any restrictions?
The SDK version used is 5.4.70 2.3.0.

Best regards,

タグ(1)
0 件の賞賛
返信
0 返答(返信)