Assistance Required for Configuring A35 Core Frequency on i.MX8QXP MEK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assistance Required for Configuring A35 Core Frequency on i.MX8QXP MEK

837 Views
mbamarnath
Contributor I

Hello Team,

I am working with the i.MX8QXP MEK and need to configure the A35 core frequency to 1 GHz from U-Boot for testing purposes. We are planning to run a set of proprietary benchmark applications on our custom RTOS, which is booted from U-Boot, and these tests need to be conducted across various operating frequencies.

Could you please advise on how I can set the A35 core frequency to a specific value from U-Boot? Any guidance or reference to the appropriate documentation for configuring the A35 CPU frequency from U-Boot would be greatly appreciated.

Thank you for your assistance.

Best regards,
Amar

0 Kudos
Reply
2 Replies

803 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For the linux you can modify in the dts file. For custom RTOS you can ask them to check on the net.

0 Kudos
Reply

662 Views
mbamarnath
Contributor I

Hello Rita,

Sorry for the late reply, our activities were paused for weeks.

Currently the RTOS doesn't configure any CPU frequency by itself instead it relies on the frequency set by the bootloader, in this case uboot.

So, where in u-boot are we configuring the CPU clock?

Regards,

Amar 

0 Kudos
Reply