Armhf linux for iMX6ul evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Armhf linux for iMX6ul evk

1,926件の閲覧回数
ATAineri
Contributor III

Good afternoon. I need to make armhf linux for iMX6ul. When I bitbake image-core-base, then "uname -a" command return that system has armel architecture and noway to install armhf package with apt-get. How can I configure bitbake to create the armhf linux with frame-buffer, but without x-server or wayland.

I thought that iMX6ul is armhf CPU...

ラベル(4)
0 件の賞賛
返信
1 返信

1,814件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Vladislav Redin,

Armhf is a Debian port, you can find more information below:

https://www.debian.org/ports/#portlist-released

The BSP release is not based on Armhf but there is a demo which may help. You can find more information on the Community Document below (please download the attachment as it contains the document with instructions and some .deb files)

https://community.nxp.com/message/323514

I hope this helps!

Regards,

0 件の賞賛
返信