Arduino header on i.MX6UltraLite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Arduino header on i.MX6UltraLite

跳至解决方案
1,872 次查看
giulianofranche
Contributor II


Hi

we would like to test the i.MX6UltraLite, but we have a pretty simple question: do we have to solder anything in the arduino header to plug some shields in?

The picture of the board shows that the JTAG connector is in the arduino header area, and I'm afraid I may not have enough space to plug the shield directly on the board

Regards

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,727 次查看
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,727 次查看
giulianofranche
Contributor II

Thank you for your answer Artur.

Do we must solder the extenders, or is this optionnal?

0 项奖励
回复
1,728 次查看
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

0 项奖励
回复
1,727 次查看
art
NXP Employee
NXP Employee

Yes, you can solder some connector extenders into the Arduino header pads to leave more space under the shield.

Best Regards,

Artur

0 项奖励
回复