Arduino header on i.MX6UltraLite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Arduino header on i.MX6UltraLite

ソリューションへジャンプ
2,011件の閲覧回数
giulianofranche
Contributor II


Hi

we would like to test the i.MX6UltraLite, but we have a pretty simple question: do we have to solder anything in the arduino header to plug some shields in?

The picture of the board shows that the JTAG connector is in the arduino header area, and I'm afraid I may not have enough space to plug the shield directly on the board

Regards

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,866件の閲覧回数
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,866件の閲覧回数
giulianofranche
Contributor II

Thank you for your answer Artur.

Do we must solder the extenders, or is this optionnal?

0 件の賞賛
返信
1,867件の閲覧回数
art
NXP Employee
NXP Employee

This is optional and use case dependent.

Best Regards,

Artur

0 件の賞賛
返信
1,866件の閲覧回数
art
NXP Employee
NXP Employee

Yes, you can solder some connector extenders into the Arduino header pads to leave more space under the shield.

Best Regards,

Artur

0 件の賞賛
返信