Application installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application installation

1,130件の閲覧回数
rizwan_s
Contributor II

HI All,

In android ,there are many applications like clock , calender ,settings etc which installs before home screen comes up.

Is it possible to install other application in Android 5.0 before  home screen come sup?

Thanks and regards

Rizwan Syed

ラベル(1)
0 件の賞賛
返信
1 返信

1,067件の閲覧回数
art
NXP Employee
NXP Employee

Do you mean launching a custom application during Android boot? If so, it is just a regular Android operation, refer to the following section on the Android Developer's web site:

https://developer.android.com/training/basics/activity-lifecycle/index.html

Also, refer to the following community thread:

https://community.nxp.com/thread/433021

Hope it would be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信