Application installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Application installation

1,122 Views
rizwan_s
Contributor II

HI All,

In android ,there are many applications like clock , calender ,settings etc which installs before home screen comes up.

Is it possible to install other application in Android 5.0 before  home screen come sup?

Thanks and regards

Rizwan Syed

Labels (1)
0 Kudos
Reply
1 Reply

1,059 Views
art
NXP Employee
NXP Employee

Do you mean launching a custom application during Android boot? If so, it is just a regular Android operation, refer to the following section on the Android Developer's web site:

https://developer.android.com/training/basics/activity-lifecycle/index.html

Also, refer to the following community thread:

https://community.nxp.com/thread/433021

Hope it would be helpful.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply