Ap6275P BT failed to receive file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Ap6275P BT failed to receive file

2,060 次查看
zhou1211
Contributor II


The platform I am using is imx8qxp

Linux version 5.10.72
Android11
 Bluetooth module is Ap6275P.

We can send files normally, and the corresponding log is BT_send.txt.

But we were unable to successfully receive the file,After receiving a portion of the files, the progress bar does not change.and the corresponding log is BT_recv.txt.

 

DTS

&lpuart1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpuart1>;
status = "okay";
 
bluetooth {
compatible = "brcm,bcm4362a2";
pinctrl-0 = <&pinctrl_bt>;
pinctrl-names = "default";
max-speed = <2000000>;
shutdown-gpios = <&lsio_gpio0 13 GPIO_ACTIVE_HIGH>;
host-wakeup-gpios = <&lsio_gpio0 16 GPIO_ACTIVE_LOW>;
device-wakeup-gpios = <&lsio_gpio0 19 GPIO_ACTIVE_HIGH>;
brcm,bt-pcm-int-params = [01 02 00 01 01];
};
};


pinctrl_lpuart1: lpuart1grp {
fsl,pins = <
IMX8QXP_UART1_TX_ADMA_UART1_TX 0x06000020
IMX8QXP_UART1_RX_ADMA_UART1_RX 0x06000020
/*Don't need en uart
IMX8QXP_UART1_RTS_B_ADMA_UART1_RTS_B 0x06000020
IMX8QXP_UART1_CTS_B_ADMA_UART1_CTS_B 0x06000020
*/
>;
};

 

[14100.679223] Bluetooth: hci0: zhq Frame reassembly failed (-90)
[14100.689458] Bluetooth: hci0: zhq Frame reassembly failed (-84)

 

 

 

 

0 项奖励
回复
2 回复数

2,043 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Seems this is the issue of this BT ship. You may need to consult the company of this wifi/bt chip.

0 项奖励
回复

1,945 次查看
zhou1211
Contributor II
The measured signals of the module are all normal. We used a logic analyzer to capture 3% of the waveform of the received file. It seems that after receiving 3%, RTS did not decrease. Do you have any modifications regarding this phenomenon.
BT_err_3.png
0 项奖励
回复