Anyone facing difficulties in Crosscompiling ICU library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Anyone facing difficulties in Crosscompiling ICU library

1,651 次查看
chandraevolute
Contributor V

Here is the solution

1. Download the source from ICU website

2. untar the source to say /linux/icu/

3. First make a copy of the source cp -rfd /linux/icu/source /linux/icu/pre_build

4. Now go to cd /linux/icu/pre_build/source do ./configure and make

5. Compile for the current OS

6. Now go to cd /linux/icu/source

7. ./configure --prefix=/home/linux/ICU/icu/source/OUT --enable-tests=no --enable-samples=no --with-cross-build=/linux/icu/pre_build/source --build=i686-linux --host=i686-pokysdk-linux --target=arm-poky-linux-gnueabi --prefix=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr --exec_prefix=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr --bindir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi --sbindir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi --libexecdir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/libexec/arm-poky-linux-gnueabi --datadir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/share --sysconfdir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/etc --sharedstatedir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/com --localstatedir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/var --libdir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/lib/arm-poky-linux-gnueabi --includedir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/include --oldincludedir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/Usr/include --infodir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/share/info --mandir=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/share/man

8. make

Now your ICU is cross compiled.

标签 (3)
0 项奖励
回复
0 回复数