Any minimal Ubuntu release available?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any minimal Ubuntu release available?

1,696 Views
Albert1z
Contributor II

Hi imx53 experts,

 

I am pleased with the pre-loaded Ubuntu running on my QuickStart board. However, I would like to start with a minimal Ubuntu system and add only the necessary software components myself to reduce bloat. May I know if such a minimal Ubuntu system is available for download? Or can I build it myself from source code?

 

Thank you.

Labels (1)
0 Kudos
Reply
2 Replies

1,604 Views
jhollister
Contributor II

The out-of-the-box configuration of the LTIB tool in the Ubuntu-based development VM (IMX_QSB_UBUNTU_VM) will generate a minimal Linux installation for the QSB. The resulting installation won't have a window manager so you'll be interacting with it through the debug serial port at first.

0 Kudos
Reply

1,604 Views
JohnReed
Contributor I

Albert,

 

Follow the directions in my post that follows yours:  "User experience with 1109 binaries ....."

It's a pretty minimal ubuntu installation, using the matchbox window manager instead of gnome.    You can start there, and then add files from the full release to get something to your liking.

 

JR

0 Kudos
Reply