Animation QML application make large load of CPU core I.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Animation QML application make large load of CPU core I.MX6

7,726 次查看
dmitrypozhidaev
Contributor III

I have embedded device with Freescale I.MX6 SoC.  I compile Qt5.3.1 from source with support OpenGL and when I run my application I have very large use cores of I.MX6 instead use GPU at max. Other more complex animations use core of CPU even greater. Look at the htop screenshot. If I build my QML application for Windows Angle CPU of PC load at 2...3% -  GPU works at maximum.  Does works OpenGLat I.MX6 correctly or for embedded Qt is it normally (i mean great load core CPU)?

The Linux kernel is 3.10.17

Source of test application:

import QtQuick 2.2

import QtQuick.Window 2.1

import QtQuick.Controls 1.2

import QtQuick.Controls.Styles 1.2

Window {

visible: true

width: 360

height: 360

MouseArea {

  anchors.fill: parent

  onClicked: {

   Qt.quit();

  }

}

ProgressBar {

  anchors.fill: parent

  anchors.margins: 40

  indeterminate: true

  style: ProgressBarStyle {

   background: Rectangle {

    radius: 2

    color: "lightgray"

    border.color: "gray"

    border.width: 1

    implicitWidth: 200

    implicitHeight: 24

   }

   progress: Rectangle {

    border.color: "steelblue"

    color: "lightsteelblue"

    // Indeterminate animation by animating alternating stripes:

    Item {

     anchors.fill: parent

     anchors.margins: 1

     visible: control.indeterminate

     clip: true

     Row {

      Repeater {

       Rectangle {

        color: index % 2 ? "steelblue" : "lightsteelblue"

        width: 20 ; height: control.height

       }

       model: control.width / 20 + 2

      }

      XAnimator on x {

       from: 0 ; to: 40

       loops: Animation.Infinite

       running: control.indeterminate

       duration: 600

      }

     }

    }

   }

  }

}

}

screenshot.png

标签 (4)
标记 (4)
12 回复数

5,805 次查看
mralmond
Contributor II

I have a similar problem on my i.core M6 (single core).

If I run a very simple qml "infinite" animation (for example a "spinner" animation or an opacity animation) the cpu temperature reaches the critical threshold (90°C) and then the kernel set the GPU speed to 1/64 until the temperature is lower.

I'm using Qt 5.0.1 and kernel 3.0.35.

Normally the temperature is around 65°C.

How can I solve this problem.?..it seems very strange...

0 项奖励
回复

5,805 次查看
caiopereira
Contributor III

Hi, I have the same problem with my compilation

I'm using Toradex Colibri IMX6 Solo 256MB so I tested with my own distro/image using Yocto 1.7 the cinematic experience consume ~ 70% CPU

Using the BSP from toradex (Openembedded) the Dizzy version consume ~52% CPU 18% Mem and the Fido ~50% 18%Mem.

I don't know what I doing wrong in my distro/image.

But 54% CPU running only Cinematic experience I think this is too much high, is this normal?

Thank you!

Best Regards,

Caio Pereira

0 项奖励
回复

5,805 次查看
dmitrypozhidaev
Contributor III

If the radiator is present, it is possible you have a bad heat transfer from the body of the chip to the heatsink

0 项奖励
回复

5,805 次查看
mralmond
Contributor II

I'm using a single core i.mx6 and unfortunately I can't mount an heatsink.

The very strange thing is that such simple animations can raise the temperature that much...are there suggestions from freescale?

0 项奖励
回复

5,805 次查看
dmitrypozhidaev
Contributor III

hi

I has same problem.When using animation power consumption increases by 5 watts. I used the radiator.

0 项奖励
回复

5,805 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Could you please provide more information on what BSP version you are using. Is it X11 or EGLFS backend?

Tried QML based applications built with Yocto project, and GPU is fully utilized.

Best regards!

/Carlos

0 项奖励
回复

5,805 次查看
dmitrypozhidaev
Contributor III

Hello, Carlos! Thank you for your answers!

My board is var-som-mx6 quadro of the variscite. File system built by buildroot 3.10.17.

Backend is EGLFS. No X11. When I run QML animation I see increase power consumption up to +5 watts. I think this is due to the activation of GPU.

Tell me please how loaded your board cpu cores when you run QML animation?

Best regards!

0 项奖励
回复

5,805 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

They have mentioned that on Cinematic Experience is 10 to 20% and wiggly is 12% CPU.

Hope this will be useful.

Best regards!

/Carlos.

0 项奖励
回复

5,805 次查看
dmitrypozhidaev
Contributor III

hi, Carlos!

Thank you for your answer. I am sorry but if possible say me - 10...20% is it summary(total) load for CPU(for 4 cores) or load of single core of quadro cores CPU?

0 项奖励
回复

5,805 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

It is total load (top).


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,805 次查看
dmitrypozhidaev
Contributor III

Thank you! It is same as i have. But it is a bit sadly.

0 项奖励
回复

5,805 次查看
CarlosCasillas
NXP Employee
NXP Employee

Hi,

We are reviewing your request internally, you will get an update soon. 

Best regards!

/Carlos

0 项奖励
回复