Android porting on imx6 solo based custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android porting on imx6 solo based custom board

890 次查看
anupamnalgundwa
Contributor I

Hi i am trying to port android on my custom board i am using l5 system image and its u image.

my kernel stars and then it try to call init but it gives error .:below is what i am getting.

EXT3-fs (mmcblk0p2): using internal journal
EXT3-fs (mmcblk0p2): recovery complete
EXT3-fs (mmcblk0p2): mounted filesystem with ordered data mode
VFS: Mounted root (ext3 filesystem) on device 179:2.
devtmpfs: error mounting -2
Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
Rebooting in 5 seconds..
mxc_restart: Watchdog reset failed to assert reset.

after that nothing happens it dont move forward

0 项奖励
回复
0 回复数