Android on IMX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android on IMX25

1,808件の閲覧回数
Sridevi_IMX
Contributor I

Hello all,

 

I would like have Android on IMX25, could you please let me know if there is a readily available Android package for IMX25.

 

If not, any one of you tried doing this, could you please let me know the steps to do this porting ?

Can you also please share the source (if you don't mind)

 

Thanks,

Senthil

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,707件の閲覧回数
nagai
Contributor I

Hi

One of board has been running android 2.1 or 2.2.

It is open source code so you may be able to get kernel source from below page and get kernel config file.

http://armadillo.atmark-techno.com/howto/try-android-on-armadillo440

 

This page support japanese only so you can get source from "Appendix 1:".

 

Bye!

0 件の賞賛
返信

1,707件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Hi.

 

Android on iMX25 are not supported by FSL. But I beleive you can port it by yourself.

 

Do you know if iMX25 hardware is enough for Android version you want?

 

You will need to get a kernel source code with android support (I think every 2.6.35 released has) and imx25 support (you can see it under menuconfig)

 

Once you have a pure linux up and running, you should configure your kernel with some Android variables. Then rightly configure PMEM initialization under arch/arch/mach-mx25/board_mx25.c

 

It should be enough for the beginning. You can try to build the android tine build, that will load only sh.

 

Before that, you should take care of ums, vold, media server, and any "feature" you want to enable for your system.

 

You can also ask for specific help here: http://groups.google.com/group/android-porting

0 件の賞賛
返信