Android on IMX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Android on IMX25

1,759 Views
Sridevi_IMX
Contributor I

Hello all,

 

I would like have Android on IMX25, could you please let me know if there is a readily available Android package for IMX25.

 

If not, any one of you tried doing this, could you please let me know the steps to do this porting ?

Can you also please share the source (if you don't mind)

 

Thanks,

Senthil

Tags (1)
0 Kudos
Reply
2 Replies

1,658 Views
nagai
Contributor I

Hi

One of board has been running android 2.1 or 2.2.

It is open source code so you may be able to get kernel source from below page and get kernel config file.

http://armadillo.atmark-techno.com/howto/try-android-on-armadillo440

 

This page support japanese only so you can get source from "Appendix 1:".

 

Bye!

0 Kudos
Reply

1,658 Views
daiane_angolini
NXP Employee
NXP Employee

Hi.

 

Android on iMX25 are not supported by FSL. But I beleive you can port it by yourself.

 

Do you know if iMX25 hardware is enough for Android version you want?

 

You will need to get a kernel source code with android support (I think every 2.6.35 released has) and imx25 support (you can see it under menuconfig)

 

Once you have a pure linux up and running, you should configure your kernel with some Android variables. Then rightly configure PMEM initialization under arch/arch/mach-mx25/board_mx25.c

 

It should be enough for the beginning. You can try to build the android tine build, that will load only sh.

 

Before that, you should take care of ums, vold, media server, and any "feature" you want to enable for your system.

 

You can also ask for specific help here: http://groups.google.com/group/android-porting

0 Kudos
Reply