Android build for MCIMX6Q-SDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Android build for MCIMX6Q-SDB

897 次查看
Gandalf-kern
Contributor IV

Which of these two builds work correctly on the MCIMX6Q-SDB, or which is the correct BSP?

sabreauto_6q i.MX 6Quad Auto Infotainment

sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform

These are taken from the android_L5.0.0_1.0.0-ga_... published/Android User's Guide.

0 项奖励
回复
1 回复

815 次查看
Yuri
NXP Employee
NXP Employee

Hello,

MCIMX6Q-SDB relates to sabresd_6dq i.MX 6DualQuad SABRE Board and SABRE Platform.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------